Options on the General tab
The following table shows the options on the
General
tab.Options | Descriptions |
|---|---|
Display chart title | Select the check box, and type up to 80 characters in the box provided. The title includes your text and the current date. The chart title shows at the top of the chart at runtime. |
Data server | Select a server to provide data to the trend.
|
Display progress bar while loading historical data | Select this check box to show progress bar with a Cancel button while loading data into the trend. This option allows operators to cancel a request for data at runtime. |
Chart style | Determines the plotting style of the chart. A trend chart can plot values against time, or against a selected pen. |
Standard | Each pen is plotted against time in a standard line chart. |
XY plot | Each pen is plotted against a selected pen, which serves as the x-axis. To use the option, add a pen under the Pens tab, click Apply , and then select the pen from the X-Axis pen list. |
X-Axis pen | Serves as the x-axis in an XY plot. |
Chart update mode | Select one of these options:
|
Manual | This option is only available when the Data Server is set to None . It does not apply when using the Real-time data server , or Poll historical data .In Manual mode, the data server sends data to the chart using the NewData method (part of the Trend object model). The NewData method can send accumulated batches of data to the trend in bursts, allowing points to be logged more frequently than once every 50 milliseconds. The data server manages the chart timing, maintains control over the timestamps, and sends the trend an array with new data for each point at the intervals specified in the NewData method. The intervals indicate the spacing of the data in the array. |
Automatic | Use this chart mode when you want the trend to update at regular time intervals. |
Refresh Rate | In Automatic mode, the Refresh Rate specifies how often the chart acquires data. The refresh rate limits are 50 milliseconds to 596 hours. Do not make the refresh rate faster than the rate at which data is updated in the data server, or OPC server. |
On Change | Use this chart mode when you want the trend object to update as data values change. In On Change mode, current data updates in the trend chart immediately, as the values change. Specify On Change mode when working with data that changes infrequently. Set the trigger for updates using either a heartbeat rate, or a deadband percentage.This option is not available when the Data Server is set to Poll historical data . |
Heartbeat | Specifies the maximum amount of time between updates. If the value of a pen has not changed within the amount of time specified, the chart shows the current value. Setting the heartbeat rate to 0 disables the heartbeat. |
Deadband | Specifies a percentage, by which a value must change before the chart shows the next value. Setting the deadband rate to 0 updates the chart whenever the value changes. |
Provide Feedback