Delete a template (TrendPro)
Delete a template at runtime or from the
FactoryTalk View Studio
Explorer window at design time.
TIP:
At runtime, the security permission
TrendPro: Delete Template
is required to delete a TrendPro template.Use the
Security Settings
dialog box to configure the permission. In the Explorer window, right-click the appropriate application or area and select Security
.To delete a template at runtime
- At runtime, on the toolbar, clickDelete Template
. - In theDelete Templatedialog box, select one or more templates and clickDelete.
Provide Feedback