General runtime settings (TrendPro)
Use the tab to set up which settings are available to operators at runtime. To prevent operators from changing these options, the tab is not available at runtime.
The following table shows settings on the tab.
Settings | Description |
|---|---|
Trend Setup | Click the button to open the Properties dialog box and configure the detailed trend appearances and behaviors at runtime.The Properties dialog box is also available at runtime if the Context menu option is enabled. |
Chart | Specify which trend panes are displayed and whether the context menus are available to operators at runtime. The panes include Tag explorer , Toolbar , Timebar , Context menu , Tag list , and Event list . You can also specify the icon size on the toolbar, or whether to collapse the tag explorer, tag list, or event list when the trend first runs. |
Properties dialog | Specify which trend property tabs are available to operators at runtime. By default, the runtime properties dialog box includes the General and Traces tabs. The General tab includes Time Period , Application , Chart , Retrieval , X-Axis , and Shape .Tip : To show Shape on the General tab at runtime, you need to select the Shape check box at design time and create a shape on the trend at runtime. |
Provide Feedback