Event list
The event list displays the list of operator actions and alarm events that have
occurred within the current trend time period. Some events may not be visible on the
chart because they are drawn behind higher priority events.
TIP:
The columns shown may vary depending on whether you are using the local or
network application.
Right-click the list to show the context menu for configuring column
settings.
The following table describes columns for the events.
Column | Description |
|---|---|
Priority | An icon that represents the urgency of the event. |
Alarm State | An icon that represents the change in alarm state caused by an
alarm event. |
Event Time | The time at which the diagnostic information occurred or the
alarm condition changed into the currently displayed state. You
can click this column to sort the list. |
Source | The name of the alarm, or the software product that generated the
diagnostic message. |
Location | The computer name from which the message generated |
Condition Name | A name that describes the alarm condition. Condition names vary
by event category. For example:
|
Message | The text that describes the operator action or alarm event. |
Resource | The name of the hardware or software object that is the subject
of the diagnostic message. |
User Name | The login ID of the user logged on to the computer when the
message was generated. |
Current Value | The value of the tag that is being monitored for alarms when the
alarm condition changed state. |
Limit Value | An integer value that specifies the limit value of the
alarms. |
Provide Feedback