Stack axes (TrendPro)
Stacking axes displays all traces on the plot surface in their own grid, or zone. Each trace will have its own y-axis visible in a shared manner along the normal x-axis. All of the axes can still be moved.
To stack the axes
- Right-click the plot surface, selectTag Axes > Stack, and select one of the following:
- Y-Axes.If more than one trace exists, displays each trace separately in its own grid.TIP:Alternate method for stacking the y-axes:On theTrendProtoolbar, clickStack Tag Y-Axes
. - X-Axes.If more than one time period exists, displays each time period separately along the x-axis.
- Both.If more than one trace and time period exists, displays each trace and time period separately.
Provide Feedback