Manually move axes (TrendPro)
You can manually move the x-axis or y-axis.
To manually move the axes
- On the plot surface, hover over the x-axis or y-axis until a separator icon displays:
. - Drag the axis to the new location. If you have multiple traces, you can drag each one to a new location.
Provide Feedback