Retrieval page (TrendPro)
How do I open the
Retrieval page (Properties dialog box)?
- On thePropertiesdialog box, click theGeneraltab.
- ClickRetrievalin the left pane.
Trend
can retrieve and plot data using the properties on this page
. The following properties are applied immediately to the current trend.The following options are available:
Options | Description |
|---|---|
Retrieval mode | Select one of the following options:
|
Display | Click the Show retrieval information on the trend checkbox. When selected, the current retrieval setting displays as a link in the upper right corner of the plot surface. |
Provide Feedback