Add traces at runtime (TrendPro)
At runtime, you can add a trace as a tag to the trend. Traces added at runtime are not
saved.
For each trace on a TrendPro object, samples are plotted using a horizontal
x-axis representing time and a vertical y-axis representing the value.
TIP:
To show data from FactoryTalk View SE data logs, make sure the data log models are started. Otherwise, the trend will not show any value of your selected tags.
To trend historical data in
a FactoryTalk Historian
SE server, Asset Framework server, FactoryTalk Historian ME module, or PI Server
, you
need to install FactoryTalk Historian Connectivity
from the FactoryTalk View
installation package on the FactoryTalk View Studio or SE Client computer.All clients must use either the same computer name or the same IP address. If you add or delete a PI server, restart your FactoryTalk View Studio or FactoryTalk View SE Client to take effect.
To add traces to a trend at runtime from the chart
- On theTag Explorerpane of the chart, expand the tree and navigate to the folder for the data source that you want to trend.
- On theItemspane, drag one or more tags to the chart.
To add traces to a trend at runtime from the context menu
- On the chart, right-click and selectProperties.
- On theTracestab, click
. - On theTag Explorerpane, expand the tree and navigate to the folder for the data source that you want to trend.
- On theItemspane, select one or more tags.
- ClickOK.
Provide Feedback