Runtime Security dialog box
How do I open the Runtime Security dialog box?
In FactoryTalk View Studio, click
Settings
> Runtime Security
.Use the
Runtime Security
dialog box to grant or deny users or groups access to the runtime application.Setting | Description |
|---|---|
Security Accounts | Opens the Security Settings dialog box. |
Account ID | The username as specified in FactoryTalk Security. |
Login Macro | The macro name or command. The macro will run every time the user logs into the application. Note: The maximum input command length is 260 characters. If the input command exceeds this length, the command is truncated and may not be executed at runtime.Login Macro box. |
Logout Macro | The macro name or command. The macro will run every time the user logs out of the application. Note: The maximum input command length is 260 characters. If the input command exceeds this length, the command is truncated and may not be executed at runtime.Logout Macro box. |
Provide Feedback