Recipe dialog box
The following table shows options in the dialog box.
Options | Description |
|---|---|
Recipe File | This displays the same recipe name as the Recipe field in the graphic display. You can type another or choose one from the list. |
When you have a recipe object on a display and the on-screen keyboard is turned on (either in the
Display Settings
- Behavior
tab or in the FactoryTalk View SE Client), if you set the focus on the recipe object and then click it, the keyboard is displayed, rather than a drop-down list of recipes.Provide Feedback