CSV file structure of recipes
The CSV files used to import recipes must be correctly formed and contain the correct fields.
The following table shows the basic structure for a CSV file.
Row | Description |
|---|---|
Header row | Required. Contains the name of the recipe description field. The value must be Description . |
Header row | Required. Contains the description for the recipe. Use a blank line if the value is empty. |
Header row | Required. Contains the names of each ingredient field. The value must be Ingredient Name,Type,Unit,Min,Max,Tag Set,Recipe
Value . |
Ingredients data rows | Required. Each row contains recipe values of each ingredient. The values must be separated by commas and must match the type of the ingredient fields. Note: Avoid blank lines in the ingredients data rows. All ingredients after the blank line will not be imported. |
The following table shows the ingredient fields.
Field | Description |
|---|---|
Ingredient Name | Required. Specify a unique name for the ingredient. Examples might be Sugar , Nitric acid, Secret sauce , 55mm carriage bolts and so on. |
Type | Required. The value must be Number or String .
|
Unit | Optional. Specify the unit for the ingredient. |
Min | Optional. Specify the minimum recipe value. This is only available for the Number
type. |
Max | Optional. Specify the maximum recipe value. The maximum value must be greater than the
minimum value. This is only available for the Number type. |
Tag Set | Required. Specify the tag name associated with the data value for the ingredient. |
Recipe Value | Required if the type is Number .Specify the data value of the tag associated with the ingredient. If the
Min and Max values are specified, the recipe value must be within
the range of the Min and Max values, otherwise the ingredient values
of the recipe file cannot be downloaded. |
Example:
The following example shows the data of a recipe file,
Chocolate.csv
.Description
Example of Chocolate recipe
Ingredient Name,Type,Tag Set,Recipe Value
Flour,Number,Cookie\material 1,0
Butter,Number,Cookie\material2,1885.9
Salut,Number,Cookie\material3,45.9
Baking_Soda,Number,Cookie\material4 ,91.8
Sugar,Number,Cookie\material5,642.9
Sugar_Brown,Number,Cookie\material6,1102.1
Egg_Powder,Number,Cookie\material7,183.7
Water,Number,Cookie\material8,113.3
Vanilla,Number,Cookie\material9,115.5
Chocolate,Number,Cookie\material10,0
Ginger,Number,Cookie\material 11,0
OAT_Flour,Number,Cookie\material12,0
Secret,String,Cookie\recipe,OAT Meal
Provide Feedback