Configure DataLogPro
Use the
DataLogPro
editor to configure tags for logging. You configure logging per tag or per log group.To configure DataLogPro
- In the FactoryTalk View StudioExplorerwindow, open theData Logfolder, and then open theDataLogProeditor.
- Open the Tag Browser on the side bar, and then select tags for logging.TIP:To select multiple tags, pressCtrlorShift.If you try to add tags from the local KEPServer Enterprise OPC server, the Tag Browser cannot browse any tags. In such cases, you should also configure DCOM.For instructions, see Set DCOM configuration for KEPServer Enterprise.
- (optional) Select the plus sign in theLog groupspane or theNew Groupicon on the menu bar to create a log group.TIP:To add tags to the log group, drag them to the group or select the plus sign in front of any tag. You can also drag tags from one group to another. After that, the tags will inherit the trigger properties of that group.To remove a tag, select it, and then click
on the far right of the table. - Make sure the log group is selected, openGroup propertieson the side bar, and then specify how data logging will be triggered.
- SelectSaveon the menu bar, and then close the editor.
Provide Feedback