Options in the Multiple Import File dialog box
The following table shows options in this dialog box.
Options | Description |
|---|---|
Select the multiple display batch import file | Select the batch import XML file you intend to use to import graphic XML files. |
Create new objects on the display | Choose this option if the XML files in the batch file are intended to create new objects on the displays. |
Update existing objects on the display | Choose this option if the XML files in the batch file are intended to modify the properties of objects already on the displays. |
Provide Feedback