Global Object Parameter Values dialog box
The following table shows options in the dialog box.
Options | Description |
|---|---|
Name | Names of global object parameters defined in the Global Object Parameter Definitions dialog box are displayed here. Users cannot edit this cell. |
Value | Type a value for the global object parameter. This can be any string. If a tag is selected in the next cell, the tag will be displayed in the Value cell. This property is optional. |
Tag | Click the browse button to open the Tag Browser and select a tag as the parameter value. Selecting a structure tag establishes a path to it that will act as the backing tag for this reference object. |
Description | The description specified in the Global Object Parameter Definitions dialog box is displayed here. Users cannot edit this cell. |
Provide Feedback