Global Object Parameter Definitions dialog box
The following table shows the options in the
Global Object Parameter Definitions
dialog box. Options | Descriptions |
|---|---|
Name | Type a tag placeholder name (for example, #1). The global object parameter must have at least a name. Global object parameter names are the same as regular parameter placeholders. This property is required. |
Description | Type a description of the parameter to provide additional information about how the parameter is used and what kind of tag should be assigned to it. For example, Assign a PID_ENHANCED tag .This property is optional. |
Provide Feedback