Advanced settings - Client window properties
The following table shows options in the page.
Option | Description |
|---|---|
Client window background color | Specify the background color on the FactoryTalk View SE Client. Click to select another color that you want in the Color palette. |
Multi-monitor | Select this option if you want to deploy the SE client on multiple monitors. |
Window size | Select the window size when it opens.
|
Show title bar | Select this if the window is to have a title bar. If this is selected and no title is specified, the default title FactoryTalk View SE Client will be displayed. |
Title bar text | Type the name that is to appear in the title bar of the FactoryTalk View SE Client at runtime. |
Show system menu and close button | Select this if the title bar is to contain a control menu icon on the left and a close button on the right. If Show title bar is not selected, this option is not available. |
Show Min/Max buttons | Select this if the title bar is to contain minimize and maximize buttons. If Show title bar and Show system menu and close buttons are not selected, this option is not available. |
Show Diagnostics List | Select this if the client window is to have a bar along the bottom of the window to display information about system activity on the FactoryTalk View SE Client computer. This information is logged by FactoryTalk Diagnostics if it has been set up to log to the Diagnostics List.At runtime, all commands issued by the FactoryTalk View SE Client that are processed on the server, are logged by FactoryTalk Diagnostics on the server computer. |
Allow undocking of Diagnostics List | Select this if the user is to be able to undock the Diagnostics List and move it elsewhere in the client window. |
The following table shows options if you select
Multi-monitor
.Option | Description |
|---|---|
Specify monitor size in pixels | To specify the width and height, enter a number between 10 and 99999. If the input value is larger than the screen resolution, the resolution value is used to show the client window. All FactoryTalk View SE Client monitors in your system must be configured with the same resolution. |
Monitors layout | Select a layout for the monitors that you plan to deploy. |
HMI server | Select an HMI server that the client will connect to. |
Display name | Type or select an initial display for the current monitor. Each monitor can have up to five initial displays. You an also set up the startup macro on the Startup components page to launch displays on multiple monitors by using monitor index parameter. |
Display parameter | Type the Display command parameters that will be used when the display is opened.For example, you can use one of the docking position parameters ( DT , DB , DL , or DR ) to attach the display to the top, bottom, left, or right edge of the FactoryTalk View SE Client window. You could also specify P , followed by a parameter file name, or T , followed by a list of parameter tags, to supply tags for a display that contains tag placeholders. |
Monitor # | Click each monitor that you plan to deploy and set up the settings. |
Dock and maximize display on a single monitor | Selecting this check box does two things:
Note : With this check box selected, if the Size to Main Window at Runtime option of Display Setting is enabled, the display's title bar will be hidden. |
Provide Feedback