Common actions in the Explorer
Some actions are common Windows actions and are not described here. The following are described because of their importance when using
FactoryTalk View Studio
.To do this | Follow these steps |
|---|---|
Open a FactoryTalk View editor | Do one of the following:
|
Open an editor’s component | Do one of the following:
|
Set up security for resources | Right-click the System folder, or a folder or icon within it, and select Security . You can then specify permissions in the Security Settings dialog box. For instructions, click Help . |
Provide Feedback