Display navigation menu at runtime
To display the navigation menu at runtime, use the
DisplayNavigationMenu
command and specify its position in the FactoryTalk View SE Client window. For the navigation menu to show as the display client starts, you can put the command in the startup macro. If you want to close and relaunch the navigation menu on the display client, you can close it by running the Abort * /D
command.
Item | Description |
|---|---|
![]() | History , Backward , and Forward buttons, which are enabled
by configuring the navigation menu appearance at design time.Use these buttons to view the history of navigated displays and go back or
forward to displays. |
![]() | Item on the navigation menu configured as shown icon only at design time. Alarms and device diagnostic event notifications can show by configuring a
folder or menu item's settings at design time. When the subscribed alarms are active, the icon of the highest priority and the
total number of active alarms show on the top right corner. When the subscribed
device is in fault, the icon and the total number of diagnostic events show on
the bottom right corner. |
![]() | Menu items on the navigation menu. |
![]() | Runtime search, which is enabled by configuring the navigation menu appearance
at design time. You can use it to locate referenced tags across all displays configured in the
current navigation menu and double-click an item to navigate to the associated
tag's faceplate or graphic display. |
![]() | Navigation menu configured as vertical that is docked on the left. You can
specify the sidebar width to show icon only or icon and text. |
Provide Feedback