HMI Server Properties - General tab
The
General
tab displays information about the HMI server. The following table shows common properties that are available for all HMI servers.
Property | Description |
|---|---|
Name | Displays the name of the HMI server that was specified when it was created. You cannot change it. |
Description | You can add text (up to 204 characters) to describe the HMI server or edit existing text if a description has been previously specified for this HMI server. |
Project file | Shows the location of the HMI server's files. |
Number of displays | Shows the number of graphic displays contained in the HMI server. |
Licensed | Shows the maximum number of graphic displays allowed by the FactoryTalk View SE Server license. This is for information only. To show the status of the HMI servers, FactoryTalk Alarm and Event servers, and data servers at runtime, add one of the following to the application:
|
Property | Description |
|---|---|
Computer hosting the server | Displays the name of the computer the HMI Server is on. To change the name of the host computer, the HMI project must exist on the computer that is going to be the host. You can type another computer name or click the browse button to search for and select one.
|
Startup Type | Select one of the following startup types to specify when the HMI server is to be loaded. If you plan to set up redundancy for the application, you must select the startup type 'Load and run startup component when operating system initializes'.
|
Provide Feedback