Command Wizard options
The following table shows options in the Command Wizard:
Options | Description |
|---|---|
Command Categories | This is a hierarchy of folders. The top folder in the hierarchy is called Most Recently Used. When you click it, the five most recently used commands are displayed in the Commands list on the right. The second folder in the hierarchy (All Commands and Macros) opens to display an alphabetical list of FactoryTalk View commands and user-defined macros. The remaining folders organize the commands by categories. When clicked, these open to display more folders, or a list of related commands. |
Name | Lists the names of the commands in the open folder. |
Description | Briefly describes each command in the list. |
Syntax | Shows the syntax for the command. Angle brackets, i.e., <file>, indicate a required parameter. Square brackets, i.e., [file], indicate an optional parameter. |
Provide Feedback