Redundancy functions
Use the redundancy functions to retrieve the server status in a redundant pair.
The server pair can be
FactoryTalk View
HMI servers, FactoryTalk Linx
servers, OPC DA servers, OPC UA servers, or FactoryTalk Alarms and Events
servers.The status value is returned as a constant integer in decimal or hexadecimal. You can then use these values to reflect different status of your servers. For example, you can create color animations or multistate indicators to show different colors, captions, or images.
The following table lists redundancy functions:
This function | Returns this value |
|---|---|
PrimaryServerStatus (ServerName ) | Returns a constant integer that presents the status of the primary server. The argument is an absolute reference to a server. It can only be a literal string with the format /AreaName/ServerName , where AreaName is the name of the area and ServerName is the name of the server. The argument must be enclosed in double quotes, for example, PrimaryServerStatus("/Area1/HMI_Demo") . |
SecondaryServerStatus (ServerName ) | Returns a constant integer that presents the status of the secondary server. The argument is an absolute reference to a server. It can only be a literal string with the format /AreaName/ServerName , where AreaName is the name of the area and ServerName is the name of the server. The argument must be enclosed in double quotes, for example, SecondaryServerStatus("/Area1/HMI_Demo") . |
Note
: In certain cases of a poor network or a large number of clients running at the same time, the returned constant may be empty or not reflect the true server status. To solve this problem, in FactoryTalk Administration Console, go to System > Policies > System Policies > Health Monitoring Policy Properties
to increase the value of computer detection interval or network failure detection interval. For more information on these policies, see FactoryTalk Services Platform Help
. Decimal | Hexadecimal | Server status | Description |
|---|---|---|---|
-2147483647 | 0x80000001 | Unknown | The server status is unknown. |
-2147483646 | 0x80000002 | Not loaded | The server is not currently in use and has not notified the system that it is running. |
-2147483645 | 0x80000003 | Failed or host unreachable | This may be one of the following:
|
-2 | 0xFFFFFFFE | Not configured | Redundancy has not been configured for a secondary server. |
1 | 0x00000001 | Loading | The server's processes are starting up, and the server is currently loading processes and components. |
2 | 0x00000002 | Starting | The server has finished loading its processes and components; it is currently reading configuration and performing other tasks in order to become available for use. |
3 | 0x00000003 | Ready to provide service | The server is ready to become the active server. |
4 | 0x00000004 | Active | The server is the active partner in an active - standby pair. |
5 | 0x00000005 | Standby | The server is the Standby partner in an active - standby pair. This state does not apply if servers are not configured for redundancy. |
6 | 0x00000006 | Active (no partner or cannot reach partner) | This may be one of the following:
|
7 | 0x00000007 | Synchronizing with Active | The server is transitioning into the Standby state. This state does not apply if servers are not configured for redundancy. |
8 | 0x00000008 | Synchronizing with Standby | The server is transitioning into the Active state. This state does not apply if servers are not configured for redundancy. |
9 | 0x00000009 | Synchronized, ready to be Active | The server is ready to become the active partner in an active - standby pair. From this state, the server transitions immediately to the Active state. This state does not apply if servers are not configured for redundancy. |
10 | 0x0000000A | Synchronized, ready to be Standby | The server is ready to become the standby partner in an active - standby pair. From this state, the server transitions immediately to the Standby state. This state does not apply if servers are not configured for redundancy. |
Provide Feedback