Alarm and Event functions
Use FactoryTalk alarm and event functions to retrieve information about a group of FactoryTalk alarms that have similar names, or about an individual alarm. These functions are available wherever expressions are supported in a FactoryTalk View SE application.
TIP:
The information returned by the FactoryTalk alarm and event functions includes
InAlarm
suppressed alarms, but does not include the other suppressed alarms.Using a large number of alarm functions can affect the performance of the system, therefore it is recommended that the total number of unique function calls accessed in displays on a FactoryTalk View SE client, should be no more than 500. Reusing the identical alarm function call does not affect performance.
For complete information about using FactoryTalk alarms and events, see
FactoryTalk Alarms and Events Help
. For an example that uses alarm expressions to animate the color of a box when the state of an alarm changes, see FactoryTalk Alarms and Events System Configuration Guide
.The following table lists Alarm and Event functions:
This function | Returns this value |
|---|---|
AE_ActiveEvents (EventName ) | A long integer from 0 to the number of server-based events that are active. |
AE_ActiveHighAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, high-priority alarms that are In Alarm and Acknowledged or In Alarm and Unacknowledged . |
AE_ActiveHighUnackedAlarms (AlarmName ) | A long integer from o to the number of FactoryTalk active, high-priority alarms that are In Alarm and Unacknowledge . |
AE_ActiveLowAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, low-priority alarms that are In Alarm and Acknowledged or In Alarm and Unacknowledged . |
AE_ActiveLowUnackedAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, low-priority alarms that are In Alarm and Unacknowledged . |
AE_ActiveMediumAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, medium-priority alarms that are In Alarm and Acknowledged or In Alarm and Unacknowledged . |
AE_ActiveMediumUnackedAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, medium-priority alarms that are In Alarms and Unacknowledged . |
AE_ActiveUrgentAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, urgent-priority alarms that are In Alarm and Acknowledged or In Alarm and Unacknowledged . |
AE_ActiveUrgentUnackedAlarms (AlarmName ) | A long integer from 0 to the number of FactoryTalk active, urgent-priority alarms that are In Alarm and Unacknowledged . |
AE_DisabledCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are disabled. |
AE_FaultedAlarmsExist (AlarmIngly ) | A Boolean representing whether any alarm exists in the Faulted state with the specified alarms, area path, or group path.Returns 0 if no alarm exists and 1 if one or more alarms exist. |
AE_HighPriorityActive (AlarmName ) | An integer from 1 to 4 representing the highest priority value associated with the specified alarms, whose states are In Alarm .
If 0 is returned, it means that none of the specified alarms were In Alarm . |
AE_HighSeverityAcked (AlarmName ) | An integer from 1 to 1000 representing the highest severity value associated with the specified alarms, whose states are In Alarm and Acknowledged . If 0 is returned, it means that none of the specified alarms were both In Alarm and Acknowledged . |
AE_HighSeverityUnacked (AlarmName ) | An integer from 1 to 1000 representing the highest severity value associated with the specified alarms, whose states are In Alarm and Unacknowledged .If 0 is returned, it means that none of the specified alarms were both In Alarm and Unacknowledged . |
AE_HistoryStatus (ServerName ) | An integer from 0 to 8 representing the connection status of the alarm history database.
|
AE_InAlmAckedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are In Alarm and Acknowledged . |
AE_InAlmShelvedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are In Alarm and Shelved . |
AE_InAlmSuppressedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are In Alarm and Suppressed . |
AE_InAlmUnackedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are In Alarm and Unacknowledged . |
AE_NormalShelvedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are Normal and Shelved . |
AE_NormalSuppressedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are Normal and Suppressed . |
AE_NormalUnackedCount (AlarmName ) | A long integer from 0 to the number of FactoryTalk alarms that are Normal and Unacknowledged . |
AE_ShelvedAlarmsExist (AlarmName ) | A Boolean representing whether any alarm exists in the Shelved state with the specified alarms, area path, or group path.Returns 0 if no alarm exists and 1 if one or more alarms exist. |
AE_UnackedAlarmsExist (AlarmName ) | A Boolean representing whether any alarm exists in In Alarm and Unacknowledged state with the specified alarms, area path, or group path.Returns 0 if no alarm exists and 1 if one or more alarms exist. |
Provide Feedback