Links dialog box
The following table shows options in the dialog box.
Options | Description |
|---|---|
Update | Select the Automatic option to update the object whenever its source file is updated, or select Manual if you want to determine when it is updated. |
Update Now | Click to update the object from its source file. |
Open Source | Click o open the application that created the object. This lets you edit the object. |
Change Source | Click this button to select another source application for the object. |
Break Link | Click to break the link between the object and its source application. After the link is broken, changes made to the source file will not affect the object. |
Provide Feedback