General line and color properties
The following table shows options on the
General
tab.Options | Description |
|---|---|
Line style | Choose a line style from these options: solid (the default), dash, dot, dot-dash and dot-dash-dash. These styles are only available when the line width is 1. |
Fore color | Displays the default or current foreground color. Click it to select another color. |
Back style | Select solid or transparent. If the back style is solid, and a line style is chosen, the back color will be visible between the dots or dashes. |
Back color | Displays the default or current background color. Click it to select another color. The background color is only visible if the Back style is solid and the Line style is a dot, dash, or a dot/dash combination. |
Line width | The line can be from 1 (the default width) to 1000 pixels wide. If it is anything other than 1, a line style is not applied if one is selected. |
Provide Feedback