Draw an ellipse or circle
Use
to draw an ellipse or circle.
to draw an ellipse or circle.To draw an ellipse or circle:
- InFactoryTalk View Studio, in the toolbox, select
. - To draw an ellipse, drag
diagonally, until the ellipse is the desired size.To draw a circle, pressCtrlwhile you drag
. - Drag the tool diagonally from one side of the object to the other. When the ellipse is the correct size, release the button.
- In theEllipse Propertiesdialog box, change the styles if needed.
Provide Feedback