Draw an arc
An arc is a segment of an ellipse's perimeter. An arc is drawn in two steps: first you create an ellipse or circle, and then you reshape the ellipse or circle.

To draw an arc:
- InFactoryTalk View Studio, in the toolbox, select
. - Drag
diagonally to draw an ellipse the size you need and then release the mouse button.TIP:To base the arc on a circle, hold downCtrlas you drag the arc tool. - In theArc Properties dialog box, make sure thatBack Styleis set toTransparent. Change other styles if needed.
- ClickOK. A set of handles appears on the object so you can reshape the ellipse.TIP:To show these handles, you can also right-click the object and selectEdit.
- Click a handle, and drag the Arc tool to cut out part of the circle.To draw the arc in 45-degree increments, pressCtrlwhile you draw.
Provide Feedback