Draw a polyline
A polyline is a series of connected line segments.

To draw a polyline:
- InFactoryTalk View Studio, in the toolbox, select
. - Drag
to create the first segment of the object. - To create the next line segment, point the tool at its end then click the left mouse button. Repeat for each line segment.TIP:To draw a horizontal or vertical line, pressCtrlas you drag the tool.
- When you finish drawing the object, double-click outside the object.
- In thePolyline Propertiesdialog box, change the styles if needed. If you choose a fill pattern, the object is filled as accurately as possible even if it is not a closed figure.
Provide Feedback