Piloted Control List Selector Properties - Timing tab
The following table shows the options in the
Timing
tab of Piloted Control List Selector Properties
dialog box.Options | Description |
|---|---|
Enter key control delay | Select the length of time to delay between the operator pressing the Enter button and the application setting the Enter control to 1. Assign the Enter control in the Connections tab. |
Enter key hold time | Select the time the Enter control will be set to 1. This time setting applies only if the Enter control is assigned and the Enter Handshake control is not assigned (in the Connections tab). |
Enter key handshake time | Select the maximum time the Enter control will be set to 1. This time setting applies only if the Enter and Enter Handshake controls are both assigned (in the Connections tab). |
Handshake reset type | Select how the Enter Handshake tag resets the Enter tag to 0:
|
Provide Feedback