Toggle Switch Properties - General tab
The following table shows options of the
General
tab.Options | Description |
|---|---|
Tag | Specify the path and name of the tag that will be the recipient of
the toggling action. |
Shape | Choose a shape for the toggle switch, rounded rectangle pill,
checkbox, or radio button. |
State: Off |
|
State: On |
|
Expression | Enter a tag name or an expression that will evaluate to True (any non-zero value) or False (zero) at runtime.An expression is a mathematical or logical equation that returns a value. It can contain tag names, constants, mathematical, relational, logical and/or bitwise operators and functions. A tag name can also stand alone as an expression. |
Expression true state | Select whether the object is in the disabled state or enabled state
when the expression returns True . |
Provide Feedback