Recipe Properties dialog box
The following table shows the options in the
Recipe Properties
dialog box.Options | Description |
|---|---|
Default recipe name | Type the default recipe name that will appear in the recipe object in the display at runtime. |
Field Length | The length displayed reflects the size of the box you drew. You can change this so that it will accommodate the recipe name. |
Justification | Choose left, center, or right justification. |
Provide Feedback