Navigation Button Properties - General tab
The following table shows options under
Appearance
of the General
tab.Options | Description |
|---|---|
Border style | Select the border style. The default style is Line. If the object is a rounded rectangle, circle, or ellipse, the available border styles are None and Line. |
Border width | Type the number of pixels for the width of the object’s border. |
Back style | Select whether the object background is solid, gradient, or transparent. If you select Transparent, the object’s background is not filled in and any objects behind it show through. If you select Gradient, the object's background is filled with a linear gradient color. If you select Solid, the background is opaque. Specify the color for the background (Back color) in the Active Appearance and Inactive Appearance tabs. |
Shape | Select the shape of the object. If the object is a rounded rectangle, circle, or ellipse, the application applies properties such as size and position by measuring in relation to the object’s bounding box. Tip : Press Ctrl while dragging a corner of the shape to form a square button. |
Corner radius | Available only when the shape is rounded rectangle. Specify how rounded you want the corners to be. |
Border uses back color | Select this check box to use the object’s background color for the border of the button. If this is not checked, you can assign a separate color to the border, instead of using the object’s background color. Specify the background color and the border color in the Active Appearance and Inactive Appearance tabs. |
Highlight color | This box displays the current highlight color. Click it to select another color in the Color palette. Click the color that you want. For button objects, the button’s border, if any, changes to the highlight color when the operator presses the button at runtime. |
The following table shows options under
Action
of the General
tab.Options | Description |
|---|---|
Action | Select one of the following options to specify the button's action:
|
The following table shows options under
Touch margins
of the General
tab.Options | Description |
|---|---|
Touch margins | Specify a touch-insensitive margin inside the button’s edges. If the operator presses on the touch-insensitive margin, the button press is not registered. |
Horizontal margin | Type the number of pixels for the horizontal touch margin. The horizontal margin is along the button’s left and right edges. |
Vertical margin | Type the number of pixels for the vertical touch margin. The vertical margin is along the button’s top and bottom edges. |
The following table shows options under
Other
of the General
tab.Options | Description |
|---|---|
Audio | Select this check box to play a sound when the object is pressed. If the computer running the project does not have audio capabilities, clicking the object does not trigger a sound. |
Provide Feedback