Options to show on-screen keyboard
Use the on-screen keyboard for applications that will be run on touch-screen terminals where keyboard input is required. The following table shows the options that FactoryTalk View SE supports to show the on-screen keyboard.
Options | Description |
|---|---|
Display On-screen Keyboard | This option applies to a numeric or string input object. You can find it in the General tab of the Numeric Input Properties or String Input Properties dialog box. |
Display On-screen Keyboard for Whole Display | The option applies to a display. You can find it in the Behavior tab of the Display Settings dialog box.It takes precedence over the Display On-screen Keyboard option. If the on-screen keyboard is turned on for a display, the on-screen keyboard will be shown for all numeric input objects, string input objects, recipe objects, or Alarm and Event objects on the current display, whether or not the individual object has been set up to show the keyboard. |
On-screen keyboard: Always use on-screen keyboard for operator entry | The option applies to a display client. You can find it in Advanced settings > other options of FactoryTalk View SE Client Wizard .It takes precedence over the other two options above. If the on-screen keyboard is turned on for a display client, the on-screen keyboard will be shown for all numeric input objects, string input objects, recipe objects, or Alarm and Event objects on any graphic display the client shows, whether or not the display or object has been set up to show the keyboard. |
Provide Feedback