Confirm Replacement dialog box
The
Confirm Replacement
dialog box opens when you select the Confirm replacements check box and click the Replace
button in the Tag Substitution
dialog box. It shows the tag or string about to be replaced, along with its usage.The following table shows options in this dialog box.
Options | Description |
|---|---|
Replace | Click this button to replace this instance of the tag. |
Next | Click this button to search for the next occurrence of the tag and display its usage in the Usage box. |
Replace All | Click this button to replace all instances of the tag in the currently selected object. |
Usage | Shows how the tag or string is being used, the type of graphic object it is associated with, and the object's position in the graphic display. |
Provide Feedback