Options on the Hyperlink tab
The following table shows options on the tab.
Options | Description |
|---|---|
Address | Specify the address that represents the linked destination. You can enter a URL address or a file path. You can also click Tag or Expression to specify a tag or an expression.An expression is a mathematical or logical equation that returns a value. A tag name can be used as an expression. |
Browse the Web | Click this button to open the default web browser on your computer. You can then
browse to the webpage that you want to link to, and copy and paste the URL to the
Address field.The URL must be enclosed in double quotes (" "). |
Browse for File | Click this button to select the file that you want to open at runtime. After you specify the file, the full path with the file name is displayed in the Address field.The path must be enclosed in double quotes (" "). |
Provide Feedback