Insert an ActiveX Control dialog box
The following table shows options in this dialog box.
Options | Description |
|---|---|
Register | If the ActiveX object you select is not registered, click this button to register it. |
Unregister | Click this button to remove the selected ActiveX object from the system registry. |
Provide Feedback