ActiveX Control Events dialog box
The following table shows options in this dialog box.
Options | Description |
|---|---|
Attach a command or macro to the event | Type a command or macro name in this field, or click the browse button (...) to open the Command wizard and use it to create a command string. |
Attach a Tag to the event’s parameters |
|
Log event to Diagnostics Log | Select the check box to log the event to the locations that are configured for the Applications category. When an event is logged, the object’s name appears in the message followed by the event name and the command. For example, the Double-click event of an RSGauge called RPM that runs the command Beep, is logged as: RPM: DblClick() Executing: Beep |
Provide Feedback