Component list file
The component list file supplied to the Add Component Tool is an XML file consisting of a list of component category headings and component file names.
The file has the following format. The
<category>
and <component>
sections can be repeating sections.<hmi> <category type="TYPE" folder="FOLDER"> <component file="NAME"/> </category> </hmi>
- TYPEis one of the component category types.
- FOLDERis the name of the folder where the component files in this category is located. This is an optional attribute. If this attribute is not present, the component files are assumed to be located in the same folder as this component list file. The folder attribute can be specified either as an absolute folder (for example,C:\SEFiles\gfx) or as a relative folder (for example,.\gfx). If it is a relative folder specification, it is assumed to be relative to the folder where this component list file is located.
- NAMEis the name of the component file without a folder specification (for example,pump.gfx).
Examples
Adding graphic displays, global object displays, and images to an existing application:
When adding graphic displays or global object displays, you can specify a folder to hold them. If the folder doesn't exist, it will create one for you.
<hmi> <category type="Graphics;Displays" folder="C:\SEFiles\Displays"> <component file="overview.gfx" folder="overview"/> <component file="pump house.gfx" folder="pumps"/> </category> <category type="Graphics;Global Objects" folder="C:\SEFiles\GOs"> <component file="button.ggfx" folder="buttons"/> <component file="panel.ggfx" folder="panels"/> </category> <category type="Graphics;Images" folder="C:\SEFiles\Images"> <component file="logo.bmp"/> <component file="pump.bmp"/> </category> </hmi>
Adding folders under Displays and Global Objects of an existing application:
<hmi> <category type="Graphics;DisplayFolders"> <component folder="line1"/> <component folder="line2"/> </category> <category type="Graphics;GlobalObjectsFolders"> <component folder="common1"/> <component folder="common2"/> </category> </hmi>
Adding XML files to an existing application:
<hmi> <category type="Graphics;Displays" folder="C:\SEFiles\Displays"> <component file="overview.xml"/> </category> <category type="Graphics;Global Objects" folder="C:\SEFiles\GOs"> <component file="common.xml"/> </category> </hmi>
Adding script files to an existing application:
<hmi> <category type="Scripts;Files" folder="C:\SEFiles\ScriptFile"> <component file="A1.ps1"/> <component file="A2.psm1"/> <component file="A3.psd1"/> </category> </hmi>
Adding a language file to an existing application:
<hmi> <category type="Language;Files" folder="C:\SEFiles"> <component file="Excelname.xls"/> </category> </hmi>
Importing FactoryTalk Alarms and Events alarms to an alarm sever
- AE area- Specifies the name of the area that contains the Tag Alarm and Event server. The syntax is<area name>/<sub-area name>, if the application type is network station or network distributed. In the case of stand-alone applications, the area name must be set to/.
- AE server- Specifies the name of the Tag Alarm and Event server.
- AE file- Specifies the full path to the XML or Excel file that contains the alarms to be imported.
- AE type- It is optional. Specifies the type of the operation. The value must be an integer from 1 through 6. If omitted, the default value is 1.
- 1. Update existing alarm definitions and create new alarm definitions from the import file.
- 2. Import only new alarm definitions from the import file and skip existing alarm definitions.
- 3. Delete all existing alarm definitions, and then create new alarm definitions from the import file.
- 4. Update existing messages and create new messages from the import file.
- 5. Import only new messages from the import file and skip existing messages.
- 6. Delete all existing messages, and then create new messages from the import file.
For a local application:
<hmi> <category type="FTAE" folder="C:\SEFiles\FTAE"> <AE area="/"/> <AE server="FTAEServer1"/> <AE file="Alarm and Event Server_AlarmImport.xml"/> <AE type="2"/> </category> </hmi>
For a network application:
<hmi> <category type="FTAE" folder="C:\SEFiles\FTAE"> <AE area="Line1_Alarms/MySubArea"/> <AE server="FTAEServer1"/> <AE file="Alarm and Event Server_AlarmImport.xml"/> <AE type="2"/> </category> </hmi>
The component category types and their associated application tree folder names are defined in the following table.
Component Category Type | Application Tree Folder Name |
|---|---|
Graphics;Displays | Displays |
Graphics;DisplayFolders | Displays |
Graphics;Images | Images |
Graphics;Global Objects | Global Objects |
Graphics;GlobalObjectsFolders | Global Objects |
Parameter;Files | Parameters |
Recipe;Files | Recipes |
RecipePro;Files | RecipePro |
MessageServer;Tables | Local Messages |
Templates;Files | Trend Templates |
TagDb;Files | Tags |
Snapshots;Files | Trend Snapshots |
TrendPro Template;Files | TrendPro Templates |
XYPlot Template;Files | XY Plot Templates |
Derived;Models | Derived Tags |
Event;Models | Events |
Macro;Files | Macros |
Key;Files | Client Keys |
Data Logging;Models | Data Log Models |
FTAE | Alarms and Events |
DataLogPro;Files | DataLogPro |
Navigation;Files | Navigation menu |
Navigation;Icons | Navigation menu |
Scripts;Files | Scripts |
Language;Files |
Provide Feedback