Enable a VPN connection
    Enter the interfaces that you want to use for establishing a VPN
      connection.
The Runtime container can establish a VPN connection with the interfaces specified in the 
VPN_ADAPTERS
 variable. Enter the interface names separated by commas. For instance: eth0,eth1,eth2
.
     NOTE: 
    If you establish a standard network bridge interface, the 
setuphost
      container creates both a tap and a bridge, if not yet in place, for each specified interface
      in the VPN_ADAPTERS
. For every tap and bridge created, the network bridge
      interface aims to append the suffixes -tap
 and -bridge
 at
      the end of the name, respectively and considering that in a Linux environment the maximum
      length for a network interface name consists of 15 characters. - Example without truncation:- Adapter name (characters length 4) =eth0
- Tap name (characters length 8) =eth0-tap
- Bridge name (characters length 8) =eth0-bridge
 
- Example with truncation:- Adapter name (characters length 9) =enp0s31f6
- Tap name (characters length 13) =enp0s31f6-tap
- Bridge name (characters length 15), note the truncation of the original name =enp0s31f-bridge.
 
Provide Feedback