Zone properties
Use zone properties to define the policy settings to apply to devices that are assigned to this zone.
Overview
The settings in this area differentiate this zone from other zones.
Property | Description |
|---|---|
Name | The name for the zone. |
Description | A description for the zone. |
Security
The settings in this area relate to how the devices in the zone communicate with other devices.
Property | Description |
|---|---|
Enable secure communication in the zone | When selected, additional configuration options for CIP Security and OPC UA are available.Non- CIP Security capable devices can be added to a zone with CIP Security enabled. These devices will have an information icon
displayed stating Incompatible with zone
configuration . These devices will not receive CIP Security policy themselves, but devices in this zone that are
CIP Security capable will add the IP address of the non-CIP Security capable device to their Trusted IP list so that
communication between the devices can occur. |
Property | Description |
|---|---|
Authentication Method | Select which method the devices use to authenticate.
Non- CIP Security capable devices do not use any authentication method. If non-CIP Security capable devices are present in a zone, an information message displays stating incompatible devices in zone when Certificate or Pre-shared Key is selected. |
I/O Data Security | Select the type of security check to perform on the input and output data.
Non- CIP Security capable devices do not use any I/O Data Security method. If non-CIP Security capable devices are present in a zone, an information message displays stating incompatible devices in zone when I/O Data Security is selected. |
Messaging Security | Select the type of security check to perform on messages received by devices in the zone.
Non- CIP Security capable devices do not use any Messaging Security and cannot provide data integrity checking. If non-CIP Security capable devices are present in a zone, an information message displays stating incompatible devices in zone when Messaging Security is selected. |
Disable port HTTP (80) | Select to disable communication over port 80.
TIP:
Not inherited by devices validated as
redundant. See Redundancy system.
|
Property | Description |
|---|---|
Inbound CIP Bridging to the backplane |
|
Outbound CIP Bridging from the backplane |
TIP:
Not available for Redundant Chassis Pairs.
See Redundancy system.
|
Property | Description |
|---|---|
Authentication method | Certificate |
For more information about
OPC UA
, see OPC UA security policy.Provide Feedback