Port properties
Devices have logical ports that are associated with IP addresses, ports, and protocols.
Some of the following properties may be read-only for:
- The devices added to the Onboarding Area by Automatic Policy Deployment.
- The devices that are not added to a secure zone.
Device
This area displays information about the device on which the port is present.
Property | Description |
|---|---|
Device name | The name of the device. Select ![]() |
Device description | Read-only information that describes the device function. |
Device catalog number | Read-only information that provides the catalog number of the device. |
For more information, see Device properties.
General
Use this area to configure the port on the device.
Property | Description |
|---|---|
Port Name | The name of the port. |
Description | The optional description for the port. |
EtherNet Driver name | A dropdown list of the available EtherNet drivers used for communication. This property is only available for the devices that support CIP Security . The default name is Ethernet .If the list does not contain a driver, add the driver with FactoryTalk® Linx™ . |
Redundancy Status | Shows the redundancy status. If available, select Validate redundancy to validate the
redundancy status for the device. |
IP Address | The IP address of the Ethernet port, for example: 10.88.11.11 You cannot edit the IP address if you:
If the Clear configuration for previous IP Address dialog appears, either:
|
Port Proxied | Appears only for proxy devices. Shows the name and the IP address of the device secured by this proxy device. Select the pencil icon ![]() |
Proxy Device | Appears only for proxied devices. Shows the name and the IP address of the device securing this proxy device. Select the pencil icon ![]() |
Policies
Use this area to select the security zone and communication settings for the port.
Property | Description |
|---|---|
Zone | The name of the zone to which the port is assigned. If Automatic Policy Deployment is enabled, the Onboarding Area displays in the list of zones. |
Disable port HTTP (80) | For CIP Security capable devices only.When a device is CIP Security capable and placed in a zone using the certificate authentication method, the HTTP Port usage can be disabled.When viewing the device list, the Disabled TCP Port column reflects whether HTTP port 80 has been disabled. |
Property | Description |
|---|---|
Model Name | The name of the policy model managed by this instance of FactoryTalk Policy Manager . |
Inbound CIP Bridging |
|
Outbound CIP Bridging |
|
Provide Feedback