Conduit properties
Use conduit properties to define the endpoints and security settings to apply to communications over this conduit. Endpoints are either a zone, a device, or a port of a device.
Each conduit must be a unique combination of endpoints.
General
Property | Description |
|---|---|
Name | Type a name for the conduit. |
Description | Type a description for the conduit. |
Connection
Property | Description |
|---|---|
Endpoint 1 | The first endpoint of the conduit. The list is composed of the zones and devices that are identified in FactoryTalk Policy Manager . |
Endpoint 2 | The second endpoint of the conduit. |
CIP Security Communication
Property | Description |
|---|---|
Authentication Method | Determines how the conduit verifies the identity of the assigned devices and/or zones.
TIP:
If an endpoint is a zone and the conduit uses certificate authentication, devices in that zone that do not support
CIP Security will not use the certificate for communication. The CIP Security capable devices will trust the non-CIP Security devices using Trusted IP. |
I/O Data Security | Determines the type of security check performed on the input and output data.
This setting is available when you choose Certificate as the Authentication Method . |
Messaging Security | Determines the type of security check performed on messages received by assets in the zone.
This setting is available when you choose Certificate as the Authentication Method . |
OPC UA
Zones and conduits follow these non-editable
OPC UA security policy
settings: - OPC UAclients trustOPC UAservers based on certificates
- OPC UAservers do not trustOPC UAservers
- OPC UAclients do not trustOPC UAclients
For more information about
OPC UA
, see OPC UA security policy.Provide Feedback