Automatic Policy Deployment notifications
FactoryTalk Policy Manager
displays the results of the Automatic Policy Deployment process in the Results
pane. If needed, you can use the following messages to troubleshoot issues with Automatic Policy Deployment.
TIP:
For detailed information about the Automatic Policy Deployment process for specific devices, see the
FactoryTalk® Diagnostics
log.New devices
Message | Description |
|---|---|
The device {name} ({IP address} ) is enrolled. The device is added to Onboarding Area. | The discovered device had no reference in the policy model and was added to the Onboarding Area. |
The Secure Onboarding Policy for device {name} ({IP address} ) was not applied. The device does not support this policy. | Automatic Policy Deployment failed to deploy the policy to the discovered device. Verify if the device supports the policy. |
The Secure Onboarding Policy for device {name} ({IP address} ) was not applied because a valid FactoryTalk Linx Driver was not found. | Automatic Policy Deployment failed to deploy the policy to the discovered device. Verify if the correct EtherNet/IP driver is assigned to the discovered device. If the driver does not exist, add the driver with FactoryTalk Linx . |
The device {name} ({IP address} ) is enrolled. The device is added to Onboarding Area. Initiating secure onboarding. | The Automatic Policy Deployment process starts. The discovered device is added to the Onboarding Area. Establishing a connection between the discovered device and FactoryTalk Policy Manager or other devices in the policy model.The deployment process completion time depends on the number of discovered devices. |
The device {name} ({IP address} ) is enrolled. The device is added to Onboarding Area. The Secure Onboarding Policy was applied. | Automatic Policy Deployment added the device to the Onboarding Area and the deployment process completed. Established a connection between the device added to the Onboarding Area and FactoryTalk Policy Manager or other devices in the policy model.You can move the device from the Onboarding Area to the policy model. |
The Secure Onboarding Policy for {name} ({IP address} ) was not applied. Check event log for more details. | Automatic Policy Deployment failed to deploy the discovered device. The discovered device was not added to the Onboarding Area. Failed to establish a connection between the device added to the Onboarding Area and FactoryTalk Policy Manager or other devices in the policy model.For more information, see the FactoryTalk Diagnostics logs. Once you resolve the issue with the device, Automatic Policy Deployment will discover and process the device again. |
The device {name} ({IP address} ) was removed from the security model. | The device that was deployed to the policy model was deleted from the policy model. Automatic Policy Deployment removed the device from the policy model. |
Devices qualified to merge
Message | Description |
|---|---|
The device {name} ({IP address} ) is enrolled and qualified as a replacement for the device {name} ({Zone name} ). All entries are merged. Initiating automatic secured device replacement. | The automatic secured device replacement process starts. The discovered device is merged with the matching device in the policy model. Establishing a connection between the discovered device and FactoryTalk Policy Manager or other devices in the policy model.The deployment process completion time depends on the number of discovered devices. |
The device {name} ({IP address} ) is enrolled and qualified as a replacement for the device {name} ({Zone name} ). All entries are merged. Policy deployment was successful. | The automatic secured device replacement process completed. The discovered device is merged with the previously deployed device in the policy model. Established a connection between the merged device and FactoryTalk Policy Manager or other devices in the policy model.If needed, you can edit the merged device properties. |
The device {name} ({IP address} ) is enrolled and qualified as a replacement for the device {name} ({Zone name} ). All entries are merged. | The automatic secured device replacement process is in progress. The discovered device is merged with the previously deployed device in the policy model. |
Policy deployment for {name} ({IP address} ) failed. Start Replace Device action manually. | The automatic secured device replacement process failed. Trying to establish a connection between the discovered device and FactoryTalk Policy Manager or other devices in the policy model.For more information, see the FactoryTalk Diagnostics logs.If needed, replace the device manually. For more information, see Devices. |
Policy deployment for {name} ({IP address} ) failed. The secure onboarding policy was not applied. The device does not support this policy. | The automatic secured device replacement process failed to deploy the policy to the discovered device. Verify if the device supports the policy. |
Policy deployment for {name} ({IP address} ) failed. The secure onboarding policy was not applied because a valid FactoryTalk Linx Driver was not found. Assign a valid driver and initiate Replace Device action manually. | The automatic secured device replacement process failed to deploy the policy to the discovered device. Verify if the correct EtherNet/IP driver is assigned to the discovered device. If the driver does not exist, you must add the driver with FactoryTalk Linx .Replace the device manually. For more information, see Devices. |
Device {name} ({IP address} ) enrolled and qualified as replacement for Device {name} ({Zone name} ). Entries merged. | The automatic secured device replacement process starts. The discovered device is merged with the matching device in the policy model. The deployment process completion time depends on the number of discovered devices. |
Deployment for {name} ({IP address} ) unsuccessful. Initiating secure onboarding. | The automatic secured device replacement process failed. Reapplying the secure policy to the device. Establishing a connection between the discovered device and FactoryTalk Policy Manager or other devices in the policy model. |
Policy for {name} ({IP address} ) deployment failed. | The automatic secured device replacement process failed. For more information, see the FactoryTalk Diagnostics logs. |
The secure onboarding policy for {name} ({IP address} ) was applied successfully. Start Replace Device action manually. | The automatic secured device replacement applied the secure policy to the device. Established a connection between the merged device and FactoryTalk Policy Manager or other devices in the policy model.Replace the device manually. For more information, see Devices. |
Deployment for {name} ({IP address} ) failed. The secure onboarding policy was not applied. Check event log for more details. | The automatic secured device replacement failed to deploy the policy to the discovered device. Failed to establish a connection between the merged device and FactoryTalk Policy Manager or other devices in the policy model.Replace the device manually. For more information, see Devices. For detailed information about the automatic secured device replacement process, see the FactoryTalk Diagnostics logs. |
Message | Description |
|---|---|
The device {name} ({IP address} ) is enrolled and qualified to merge with existing {name} ({Zone name} ) device in the model. All entries are merged. | The automatic secured device replacement process starts. The discovered device is merged with the matching device in the policy model. The deployment process completion time depends on the number of discovered devices. |
The secure onboarding policy for {name} ({IP address} ) was not applied. The device does not support this policy. | The automatic secured device replacement process failed deploy the policy to the discovered device. Verify if the device supports the policy. |
The secure onboarding policy for {name} ({IP address} ) was not applied because a valid FactoryTalk Linx Driver was not found. | The automatic secured device replacement process failed to deploy the policy to the discovered device. Verify if the correct EtherNet/IP driver is assigned to the discovered device. If the driver does not exist, add the driver with FactoryTalk Linx . |
The device {name} ({IP address} ) is enrolled and qualified to merge with existing {name} ({Zone name} ) device in the model. All entries are merged. Initiating secure onboarding. | The automatic secured device replacement process starts. The discovered device is merged with the matching device in the policy model. Established a connection between the merged device and FactoryTalk Policy Manager or other devices in the policy model.The deployment process completion time depends on the number of discovered devices. |
The device {name} ({IP address} ) is enrolled and qualified to merge with existing {name} ({Zone name} ) device in the model. All entries are merged. The secure onboarding policy was applied. | The automatic secured device replacement process starts. The discovered device is merged with the matching device in the policy model. Established a connection between the merged device and FactoryTalk Policy Manager or other devices in the policy model.The deployment process completion time depends on the number of discovered devices. |
The secure onboarding policy for {name} ({IP address} ) was not applied. Check event log for more details. | The automatic secured device replacement process failed. Failed to establish a connection between the merged device and FactoryTalk Policy Manager or other devices in the policy model.For more information, see the FactoryTalk Diagnostics logs. |
Message | Description |
|---|---|
The device {name} ({IP address} ) is enrolled and qualified as a replacement for the device {name} ({Zone name} ). All entries are merged. | The automatic secured device replacement process starts. The discovered device is merged with the matching device in the policy model. |
The device {name} ({IP address} ) is enrolled and qualified as a replacement for the device {name} ({Zone name} ). The secure onboarding policy was not applied. The device does not support this policy. | The automatic secured device replacement process was unable to deploy the policy to the discovered device. Verify if the device supports the policy. The discovered device is merged with the matching device in the policy model. |
The secure onboarding policy for {name} ({IP address} ) was not applied because a valid FactoryTalk Linx Driver was not found. Assign a valid driver and Replace Device. | The automatic secured device replacement process failed to deploy the policy to the discovered device. Verify if the correct EtherNet/IP driver is assigned to the discovered device. If the driver does not exist, add the driver with FactoryTalk Linx .Replace the device manually. For more information, see Devices. |
The device {name} ({IP address} ) is enrolled and qualified as a replacement for the device {name} ({Zone name} ). All entries are merged. Initiating secure onboarding. | The discovered device is merged with the matching device in the policy model. Establishing a connection between the device added to the policy model and FactoryTalk Policy Manager or other devices in the model.The automatic secured device replacement process starts. The deployment process completion time depends on the number of discovered devices. |
Device {name} ({IP address} ) enrolled and qualified as replacement for Device {name} ({Zone name} ). All entries are merged. The secure onboarding policy was applied successfully. | The automatic secured device replacement process completed. Established a connection between the device added to the policy model and FactoryTalk Policy Manager or other devices in the model. |
The secure onboarding policy for {name} ({IP address} ) was not applied. Check event log for more details. | The automatic secured device replacement process failed to deploy the discovered device. Failed to establish a connection between the device added to the policy model and FactoryTalk Policy Manager or other devices in the model.For more information, see the FactoryTalk Diagnostics logs. Once you resolve the issue with the device, Automatic Policy Deployment will discover and process the device again. |
Message | Description |
|---|---|
The device {name} ({IP address} ) is enrolled and qualified to merge with existing {name} ({Zone name} ) device in the model. All entries are merged. | The Automatic Policy Deployment process starts. The discovered device is merged with the matching device in the policy model. |
The secure onboarding policy for ( {name} ({IP address} ) was not applied. The device does not support this policy. | The Automatic Policy Deployment process failed to deploy the policy to the discovered device. Verify if the device supports the policy. |
The secure onboarding policy for {name} ({IP address} ) was not applied because a valid FactoryTalk Linx Driver was not found. Perform manual merge in a destination zone. | The Automatic Policy Deployment process failed to deploy the policy to the discovered device. Verify if the correct EtherNet/IP driver is assigned to the discovered device. If the driver does not exist, add the driver with FactoryTalk Linx . |
The device {name} ({IP address} ) is enrolled and qualified to merge with existing {name} ({Zone name} ) device in the model. All entries are merged. Initiating secure onboarding. | The discovered device is merged with the matching device in the policy model. The secure onboarding process starts. Establishing a connection between the device added to the policy model and FactoryTalk Policy Manager or other devices in the model.The deployment process completion time depends on the number of discovered devices. |
The device {name} ({IP address} ) is enrolled and qualified to merge with existing {name} ({Zone name} ) device in the model. All entries are merged. The secure onboarding policy was applied. | The Automatic Policy Deployment process added the device to the policy model and the deployment process completed. Established a connection between the device added to the policy model and FactoryTalk Policy Manager or other devices in the model. |
The secure onboarding policy for {name} ({IP address} ) was not applied. Check event log for more details. | The Automatic Policy Deployment process failed to deploy the discovered device. Failed to establish a connection between the device added to the policy model and FactoryTalk Policy Manager or other devices in the model.For more information, see the FactoryTalk Diagnostics logs. |
Provide Feedback