FactoryTalk System Services
FactoryTalk System Services
provide the policy authority, certificate authority, identity services, and deployment services required to enforce security policies.Databases
FactoryTalk System Services
use CouchDB for the creation and maintenance of policy databases.
TIP:
FactoryTalk System Services
depends on database services. Database services can take up to 2 minutes to start after the computer is restarted. During that time, FactoryTalk Policy Manager
will be unable to connect to FactoryTalk System Services
.During the
FactoryTalk System Services
installation, CouchDB:
- Installs automatically if not already installed.
- Adds and configures the required administrative users and controls.
- Creates policy databases.
Services
FactoryTalk Policy Manager
uses these FactoryTalk System Services
: - Authentication Service
- Authenticates users and validates user resource requests. Validates user credentials againstFactoryTalk DirectoryandFactoryTalksecurity policy settings to obtain privileges associated with the user.
- Certificate Service
- Issues and manages X.509v3 certificates for use within theFactoryTalksystem.
- Deployment Service
- Translates the security policy model defined usingFactoryTalk Policy ManagertoCIP™andOPC UAconfigurations that are delivered to endpoints. Protocols configurations are deployed independently.
- Diagnostics Service
- MakesFactoryTalkaudit and diagnostic logs available as a web service.
- Policy Service
- Builds and manages network trust models and define security policy forCIPandOPC UAendpoints.
- Differential deployment
- Enables deployment of changes in the security policy model only to the affected devices, instead of deploying the model to all devices.
- Support forCIP SecurityProxy devices
- Uses proxy devices to secure communications to and from devices that do not haveCIP Securitycapabilities.
- Backup and restore
- Preserves and restores the security policy models if there is a system failure.
- Security eventing
- Sends eventing configuration to devices and stores events fromFactoryTalk Policy ManagerandFactoryTalk System Servicesas Syslog messages.
- DTLS timeout
- Configures the devices to close their DTLS sessions after a specified period of inactivity.
Provide Feedback