FactoryTalk® Optix
Runtime Tools

You must install the Runtime Tools package on the target device to allow for entitlement management and application deployment. This package includes the following components:
  • Entitlement Manager - Application that manages
    FactoryTalk® Optix
    entitlements.
  • FactoryTalk® Optix
    Application Update Service - Service that runs in the background that connects
    FactoryTalk® Optix Studio
    to the target device so you can update and deploy
    FactoryTalk® Optix
    Applications.
  • FactoryTalk® Optix
    Runtime - Service that is optionally selected when installing the Runtime Tools on the target device. Runtime runs the
    FactoryTalk® Optix
    Application as a service on the target runtime device.
Package Components
IMPORTANT: Runtime Tools come installed in the
OptixPanel
and Embedded Edge Compute module. You must download, install, and activate Runtime Tools for
Windows®
and Linux devices.
IMPORTANT: Runtime Tools requires an entitlement that you must allocate to an organization, then assign to the devices where they are installed. See FactoryTalk Optix Runtime Entitlement.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal