Develop a button that animates an SVG image
    Configure an Advanced SVG Image object to animate the image at runtime.
     NOTE: 
    
Download a sample project:
 RotateImage.zipApplication example

Prerequisites
- To develop the project
- Arrange the interface elements.

Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback