Animate the side menu
    - Select the side menu shape, and inPropertiesselect, and select Variable. Variable.
- Rename the new variable toSideMenuActive
- Change the variable data type to Boolean.
- Select the button, and inEvents, next toMouseClick Event:- Select. 
- Select .
- ChooseSelect.
 
- InEvents, next toVariableToModifyselect. Add Dynamic Link Add Dynamic Link
- Select .
- Select the side menu, and inPropertiesnext toLeft marginselect. Add Dynamic Link Add Dynamic Link
- In theAdvancedtab, next toLeft margin:- Select. 
- SelectConditional converter.
- SetFalse valueto-140
- Next toCondition Dynamic linkselect. Add Dynamic Link Add Dynamic Link
- Select .
- SelectOK.
 
Provide Feedback