Develop an interface for switching locales
    Create a localized label and two buttons that change the interface language.
Application example - English locale

Application example - Polish locale

     NOTE: 
    
Download a sample project:
 SwitchLocales.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback