Develop a UI that generates a PDF report
    Generate a PDF report with a custom header and footer that contains information from a data grid.
Application example

     NOTE: 
    
Download a sample project:
 PDFReportWithDataGrid.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design

Report design

Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback