Add a spin box
    Create a spin box to display and control the value that determines which screen to display.
- InProject view, right-clickModeland select .TIP: Instead of adding a model variable and relying on its value, you can configure a communication driver and import a variable value from a controller. For more information, see Communication drivers.
- InProject view, right-clickMainWindow (type)and select .
- InProperties:- Create a dynamic link betweenValueand .
- SetMinimum valueto1
- SetMaximum valueto3
 
Provide Feedback