Display a dialog on value change
    Display a dialog box when variable value or tag value changes to a different value.
Application example
The panel displays when the spin box value changes.


     NOTE: 
    
Download a sample project:
 DisplayDialog.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example


Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback